LTE TDD

Full-filled Config (Advanced TDD Downlink)

For Waveform Playback (ARB) capability.

Full-filled Config sets the channels with fully filled DL-SCH configuration. The following dialog box is accessible by clicking the Full-filled Config button displayed in the toolbar when you add an Advanced TDD Downlink carrier.

SCPI Command 

[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:CONFig:FFILled <string>

SCPI Example 

:RAD:LTET:WAV:CCAR1:CONF:FFIL "SystemBandwidth: B10M, Modulation: QPSK"

Notes

Sets only (Immediate Action)  
<string>: "name:value,name:value" 

Preset 

Refer to the element definition of the data part below. 

State Saved 

No

Min

N/A

Max

N/A

Range 

Refer to the element definition of the data part below. 

Initial S/W Revision 

A.20.01 

Element definition of the data part. The preset value is basically the same as the default value of each setting definition. 

Settings 

Symbols in the data part 

Values in the data part 

Preset values 

System Bandwidth 

System Bandwidth 

B1M4 | B3M | B5M | B10M | B15M | B20M 

B10M 

Modulation 

Modulation 

QPSK | QAM16 | QAM64 | QAM256 

QPSK

 

 

Carrier Advanced TDD Downlink ARB

Welcome to LTE TDD